Common Failure: Corrosion


How do I know that my gauge is experiencing corrosion?

  • Pointer is corroded
  • Discolored liquid case fill
  • Build-up in case

What causes corrosion in my gauge?

Failure due to corrosion can be caused by several things. When looking at your system, consider the following:

  • Are contaminants getting inside of the case?
  • Is the fill plug missing?
  • Is the case or window cracked?

Possible Risks

  • Contaminants cause corrosion of the Bourdon tube
  • Contaminant inside the gauge window result in inability to read the gauge or for the gauge to show an inaccurate reading
  • System media will release into the environment resulting I potential injury and lost system media
currosion3-1

Gauges can fail due to Corrosion.

If you notice discolored liquid in the case fill, build-up in the case, or the pointer is corroded, corrosion could be an issue.

 

Break down this common failure issue:

 

Causes

Failure due to corrosion can be caused by several things. When looking at your system, consider the following:

  • Are contaminants getting inside the case?

  • Is the fill plug missing?

  • Is the case or window cracked? 

Risk

  • Contaminants cause corrosion of the Bourdon tube

  • Contaminant inside the gauge window results in the inability to read the gauge or for the gauge to show an inaccurate reading.

  • System media will be released into the environment, resulting in  potential injury and lost system media

 

Solution

Select a gauge with a liquid case fill or with a hermetical seal to keep contaminants out. Use a diaphragm seal solution in a non-316 alloy for increased corrosion resistance. 

 

Pressure Gauge Catalog

Download our Pressure Gauge Catalog for information on our product offering.